AXIS#.GEAR.DEC
Description
AXIS#GEAR.DEC defines the maximum deceleration rate the slave will follow to come out of gearing, to rest. AXIS#GEAR.DEC will only be used if Gearing is stopped for any reason, including if an AXIS#.STOP command is issued. As soon as the axis has come to rest, AXIS#GEAR.DEC will no longer be in effect and the axis will behave according to the rules of whatever motion is commanded next.
Versions
Action | Version | Notes |
---|---|---|
Implemented | 02-00-00-000 |
General Information
This content is not applicable to KAS.
Type |
Read/Write |
Units |
Rotary: RPM"Revolutions per minute" Is a unit of frequency of rotation: the number of full rotations completed in one minute around a fixed axis. It is used as a measure of rotational speed of a mechanical component/s, RPS/s, deg/s2, (custom units)/s2, rad/s2 See Acceleration Units for details. |
Range |
Depends on units. See Acceleration Range for details. |
Default Value |
10,000 RPM/s Depends on units. See Acceleration Units for details. |
Data Type |
Float |
Stored in Non Volatile Memory |
Yes |
Variants Supported
All variants are supported
Fieldbus Information
FieldbusA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design | Parameter | Index | Sub-Index | Data Type | Float Scale | Units | Access | PDO Mappable |
---|---|---|---|---|---|---|---|---|
EtherCATEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen | AXIS1.GEAR.DEC | 0x5006 | 0x2 | UDINT | - | Acceleration | RW | False |
AXIS2.GEAR.DEC | 0x5106 | 0x2 | UDINT | - | Acceleration | RW | False |